Software Version 2.14.0

General Settings

The operations that can be performed in the General Settings section are as follows:

  • Logging Level

  • Extract Log

  • Remember Window Layout

  • Default Temperature Unit

Logging Level

Based on the different Logging Levels the client and server logs can be extracted. When a logging level is set, it becomes the new default setting and any lower levels are automatically included in the extracted report.

For example: If the Information level is selected, it includes the Warning, Error and the Fatal levels. This feature might be helpful for the debugging purposes.

NOTE:
  • Click Apply to make the selected Logging Level as a user-defined

  • Click Reset to change the Logging level to the system default, which is the Information logging level

    Confirm Yes in the Confirmation dialog box.

Logging levels

Purpose

Description

Error

This is a default level and can be used in general day to day usages

This logging level is helpful when an error occurs in the software

NOTE: This is the default level set in the software

Warning

This level is used based on the need to check any warnings generated

This logging level includes any warnings generated during the configuration

Information

This level is used to capture more information details in the Client logs

This logging level includes the login and session information

Fatal

This level is used based on the need to trace a software crash

This logging level is helpful when the software crashes

Extract Log

The log events of C-Bus Commission and C-Gate can be extracted using Extract Log button.

The steps to extract logs for the specified logging level is as explained below:

  1. Select the number of days for which the Log has to be extracted and click Extract Log

    NOTE: The number of days selected will not be saved in the general settings and is only used to extract log.
  2. Save As” window is displayed

    NOTE: The details are saved in zip file.

    Click Save

Window Layout

Remember Window layout

Toggle ON, to remember the user-defined layout.

Reset Window layout

To reset the system default setting as windows layout, click Reset Window Layout

Temperature Unit

The Default Temperature unit can be set either as Celsius or Fahrenheit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.