Software Version 2.14.0

Delete Groups

The delete option allows you to delete one or more group addresses from a Lighting application.
Prerequisites: The groups must already be created in Lighting Application.
  1. Click Lighting application.
  2. Select the group address check box to be deleted in the Groups section.
    NOTE:
    • A single group can be chosen by selecting the check box of the required group, whereas all groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one group, then hold down the SHIFT key and select on additional groups (grid) using the mouse.

    • For random multiple selection, select one group, then hold down the CTRL key and select the next groups (grid) using the mouse.

    • The icon will be disabled, if a group is not selected.

  3. Click in the Groups section. A Confirmation pop-up is displayed.
  4. Click Yes to delete the group address.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.