Software Version 2.14.0

Copy Groups

The group addresses in an Application can be aligned/arranged with same addresses as in the other application.
Pre requisites: The group addresses must already be added in an Application.

In a multi-network project the group addresses of an application on a network can communicate with group addresses of an application on other network via a C-Bus bridge.

  1. Click Lighting application.
  2. Select the group address check box to be copied in the Groups section.
    NOTE:
    • A single group can be chosen by selecting the check box of the required group, whereas all groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one group, then hold down the SHIFT key and select on additional groups (grid) using the mouse.

    • For random multiple selection, select one group, then hold down the CTRL key and select the next groups (grid) using the mouse.

    • The icon will be disabled, if a group is not selected.

  3. Click in the Groups section.
    NOTE: Click in the Application section to copy the complete application.
    Step result: The selected group addresses are copied.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.