Software Version 2.14.0

Delete Test Groups

The delete function allows you to delete one or more Test Group Addresses from an Emergency Exit Light application.
Prerequisites: The Test Group Address must already be created in an Emergency Exit Light application.
  1. Select the Test Group.
    NOTE:
    • A single test group can be chosen by selecting the check box of the required group, whereas all test groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one test group, then hold down the SHIFT key and select on additional test group (grid) using the mouse.

    • For random multiple selection, select one test group, then hold down the CTRL key and select the next test group (grid) using the mouse.

  2. Click in the Test Groups section.
    A Confirmation pop-up is displayed.
    NOTE: Trying to delete the test group with existing devices associated to test group, displays a Confirmation pop-up to confirm the deletion of existing Test Group.
  3. Click Yes to delete the channels and No to cancel the delete operation.
    TIP: Alternate method to delete selected test groups is, right-click on the selected Test Group > Delete.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.