Software Version 2.14.0

Paste Levels

Prerequisites: The Levels must already be copied from a selected Group.
The Paste Level option allows the user to paste the Levels copied from one group into different group on the same network or into a Group on another network.
  1. Select the Group in the group section of the network to be pasted in
    NOTE: Levels can either be pasted on same network or into a Group on another network.
  2. Click in the Levels section.
    NOTE: The Process to Paste Levels from Excel is as demonstrated below:
    Step result: The copied Levels are pasted.
IMPORTANT: Paste conflict occurs when already existing level name and level address are been pasted in lighting application of another network.

The process to Resolve conflict is as demonstrated below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.