Software Version 2.14.0

Add Levels

Prerequisites: The Group must already be created/added in the lighting application
  1. Select a Group in the group section
    NOTE: If a group is not selected, the will be disabled.
  2. Click in Levels section
    Step result: Single Level is added for a selected group.
  3. The steps to Add Multiple Levels for a single group at a time is as demonstrated below:
    Step result: Multiple Levels are created.
  4. Level Name can be edited as demonstrated below:
    Step result: Level Name is updated.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.