Software Version 2.14.0

Firmware

Prerequisites: Make sure you have the SpaceLogic C-Bus Commission software open. Connect the C-Bus unit to your PC using the appropriate USB cable.

The Firmware section enables you to easily update the firmware of your C-Bus units. The necessary firmware files for the update process are available within the software.

To upgrade the firmware:

  1. Click .

  2. Click Firmware.

    NOTE: When no devices are connected, the Firmware upgrade page is displayed with Refresh icon enabled and Upgrade disabled.
  3. Connect a Unit device and click Refresh. Once devices are detected, Upgrade is enabled.

  4. Click the Firmware to Upload drop-down menu to change the firmware version of any connected device.

    IMPORTANT:
    • User can upgrade only one device of the same type at a time. For example, one DALI 2 Gateway at a time out of two DALI–2 Gateways.

    • User can upgrade multiple devices of different type at a time. For example, one Key Input device and one Digital Dimmer.

  5. Click Upgrade.


For product specific firmware upgrade, refer Unit type firmware upgrade.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.