Software Version 2.14.0

Copy Enable Groups

In a multi-network project, the group addresses of an Enable application on a network can communicate with group addresses of a Enable application on another network via C-Bus bridge.
Prerequisites: The enable group address must be already created in an application.

The enable group addresses in the Enable application can be aligned/arranged with same addresses as in the other Enable application.

  1. Click Applications > Enable.
  2. Select the Enable Groups check box to be copied in the Enable Groups section.
    NOTE:
    • A single group can be chosen by selecting the check box of the required group, whereas all groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one group, then hold down the SHIFT key and select on additional groups (grid) using the mouse.

    • For random multiple selection, select one group, then hold down the CTRL key and select the next groups (grid) using the mouse.

    • The icon will be disabled, if a enable group is not selected.

  3. Click in the Enable Groups section of Enable application.
    NOTE: To copy the complete application, click in the application section.
    Step result: The selected enable groups are copied.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.