Software Version 2.14.0

Levels

The Level is the value of the Group Address network variable.

Every Group Address has 256 steps between OFF (0 and 0%) and ON (255 and 100%). These 256 steps are referred to as Levels.

Levels are referred differently in different C‑Bus Applications.

When the Group Address is on the Trigger Application or Enable Application, the 256 steps in a Group Address are referred to as Action Selectors and Values respectively.

Levels and Action Selectors are most commonly used to trigger an event like a scene.

Operations performed on Levels are:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.