Software Version 2.14.0

Edit Trigger Group

Prerequisites: Make sure you have selected Trigger application and trigger groups has been created.
  1. Double-click on the trigger group name that has to be edited/renamed
    Step result: Edit Group Dialog box is displayed.
  2. Edit the Trigger Group name and click OK
    NOTE: Special characters /,”,# and maximum of 32 characters in the trigger group name are valid.
    Step result: The Trigger group name is updated.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.