Software Version 2.14.0

Add Action Selectors

The Action Selector is the value of the Trigger Group address.
Prerequisites: The Trigger Group must already be added in the application.

Each Trigger Group Address can create a maximum of 256 (0 to 255).

  1. Select a trigger group in the Trigger Group section

    NOTE: If a group is not selected, the will be disabled.

  2. Click in Action Selector section
    Step result: Single Level is added for a selected group.
  3. The steps to Add Multiple Action Selectors for a single Trigger group at a time is similar to as demonstrated in lighting application, click here
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.