Software Version 2.14.0

Add values

The Values is the value of the Enable address.

Prerequisites: The Enable Group must already be created in the Enable application.

Each Enable group Address can create a maximum of 256 (0 to 255).

  1. Select a Enable group in the enable group section

    NOTE: If a group is not selected, the will be disabled.
  2. Click and choose address in values section

    Step result: Single Value is added for a selected Enable group.

  3. The steps to Add Multiple values for a single Enable group at a time is similar to as demonstrated in lighting application, click here

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.