Software Version 2.14.0

Delete Action Selectors

The delete option allows you to delete one or more Action Selectors added to a Trigger Group address.
Prerequisites: The Action Selectors must already be created in a selected Trigger Groups address.
  1. Go to Applications > Trigger.
  2. Select the Trigger Group address check box. The Action Selectors for the selected trigger group address are displayed in the Action Selectors section.
    NOTE: When trigger group is selected, in the Action Selectors section will be disabled.
  3. Select the Action Selector to be deleted.
    NOTE:
    • A single action selector can be chosen by selecting the check box of the required action selector, whereas all action selector can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one action selector, then hold down the SHIFT key and select on additional action selectors (grid) using the mouse.

    • For random multiple selection, select one action selector, then hold down the CTRL key and select the next action selector (grid) using the mouse.

    • The icon will be disabled, if a action selector is not selected.

  4. Click in the Action Selectors section. A Confirmation pop-up is displayed.
  5. Click Yes to delete the action selectors.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.