Software Version 2.14.0

Copy Trigger Groups

In a multi-network project the Trigger Group addresses of an Trigger application on a network can communicate with Trigger Group addresses of a Trigger application on another network via C-Bus bridge.
Prerequisites: The Trigger Group address must be already created in an application.

The Trigger Group addresses in the Trigger application can be aligned/arranged with same addresses as in the other Trigger application.

  1. Go to Applications > Trigger.
  2. Select the Trigger Group check box to be copied in the Trigger Groups section.
    NOTE:
    • A single trigger group can be chosen by selecting the check box of the required trigger group, whereas all trigger groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one trigger group, then hold down the SHIFT key and select on additional trigger groups (grid) using the mouse.

    • For random multiple selection, select one trigger group, then hold down the CRTL key and select the next trigger groups (grid) using the mouse.

    • The icon will be disabled, if a trigger group is not selected.

  3. Click in the Trigger Groups section.
    Step result: The selected trigger group addresses are copied.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.