Software Version 2.14.0

Edit Test Devices

Prerequisites: The test devices must already be existing in the Emergency Exit Light application.

  1. Double-click on either CDG name, Line name, or EEL name that has to be edited.

    Step result: Edit Value dialog box is displayed.

  2. Edit the new name and click OK

    NOTE: Special characters except /,”,# and maximum of 32 characters in the Values name are valid.

    Step result: The device name is updated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.