Software Version 2.14.0

Delete Test Devices

The delete function allows you to delete one or more devices added to the Devices section.

Prerequisites: The devices must already be created in the selected Devices section.

  1. Select the devices in Devices section.

    NOTE:
    • A single device can be chosen by selecting the check box of the required group, whereas all devices can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one device, then hold down the SHIFT key and select on additional devices (grid) using the mouse.

    • For random multiple selection, select one device, then hold down the CTRL key and select the next device (grid) using the mouse.

  2. Click in the Devices section.

    A Confirmation pop-up is displayed.

  3. Click Yes to delete the devices and No to cancel the delete operation.

    TIP: Alternate method to delete selected test devices is, right-click on selected Test Device > Delete.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.