Software Version 2.14.0

C-Bus Automation Controllers

The C-Bus Network Automation Controller and C-Bus Application Controller units are DIN Rail-mounted C-Bus units. They enable C-Bus to perform complex conditional events, real-time scheduling, combinations of conditional events and scheduling, calculations, and protocol conversions. This support automation functions such as control and monitoring of C-Bus groups and scenes. The unit is programmed via its own internal web interface, which is accessible via a USB cable or an Ethernet network.

SpaceLogic C-Bus Commission supports the below automation and application controllers.

Unit Type

  • 5500NAC (PC_NAC)

  • 5500NAC (SYS_NAC)

  • LSS5500NAC (PC_NAC)

  • LSS5500NAC (SYS_NAC)

Unit Type

  • 5500SHAC (PC_SHAC)

  • 5500SHAC (SYS_SHAC)

  • LSS5500SHAC (PC_SHAC)

  • LSS5500SHAC (SYS_SHAC)

Unit Type

  • 5500AC2 (PC_AC2)

  • 5500AC2 (SYS_AC2)

  • 5500NAC2 (PC_NAC2)

  • 5500NAC2 (SYS_NAC2)

When any controller unit is added to the Devices in Project, three layers of the controller are displayed. They are IP layer, PC and SYS.

  • IP Layer will not have any address, serial, firmware version or unit type.

  • IP Layer cannot be readdressed.

    NOTE: Ensure that the PC and SYS levels are readdressed as per current implementation without losing the IP layer.
  • The SYS and PC layer are used to configure, reconcile and deploy to the device.

  • The SYS and PC layer cannot be deleted independently.

  • When loading the IP layer in Property window, the Deploy to network is disabled.

Connect to the controllers: Configure IP layer of the controllers to sync or connect to the controllers or can enter manually at the time of connection.

Controller sync functions: Controller sync consists of 2 functions:

  • Push: Push (Transfer) function is used to push the object list to the controller.

  • Pull: Pull (Retrieve) function is used to pull the data back from the controller and store data in the project.

The field information to configure SpaceLogic C-Bus Automation Controllers is explained below:

IP layer/group layer

Local Connection Service

IP Address/Host

IP address of the controller.

C-Bus Port

Default 10001.

USB IP Address

Default IP address for USB connection.

Mac Address

Mac address of the controller (read-only).

HTTP PORT

Default 80 (range restricted to 16-bit unsigned integer 0 -65535).

HTTPS PORT

Default 443 (range restricted to 16-bit unsigned integer 0 -65535).

Remote Connection Service

IP Address/Host

IP address of the remote device.

C-Bus Port

Default 10001 (range restricted to 16-bit unsigned integer 0 -65535).

HTTP PORT

HTTP port of the device (range restricted to 16-bit unsigned integer 0 -65535).

HTTPS PORT

HTTPS port of the device (range restricted to 16-bit unsigned integer 0 -65535).

Controller Configuration

IMPORTANT: Configuring of the device is done only on the Devices in Project (project database).

Controller Sync

Object List

To create object lists click .

Transfer

Retrieve

SYS_INTERFACE (NAC/SHAC/NAC2/AC2)

Global

This section allows users to check and update the C-Bus clock information.

C-Bus Clock

This check box enables/disables the resident C-Bus clock. The Enable C-Bus Clock check box is ticked (enabled) by default.

IP Address

N/A

USB IP Address

Default (read only)

Mac Address

N/A

Unit Identification

This section display the fields for identification of the unit.

Unit Type

This field contains the unit type of the device.

Firmware Version

This field shows the version number of the C-Bus interface firmware which exists on the physical network or which has been assigned to a logical representation of the unit in the database.

NOTE: For SYS_NAC/SHAC, the minimum firmware version to support is 1.14.00.

Catalogue Number

This field contains the catalog number related to the unit type.

Part Name

This field contains the part name which is stored in the unit hardware.

Unit Address

This field displays the unit address assigned to the device.

Serial Number

This field contains the serial number which exists on the physical network.

Tag Name

This field contains the name that user can give to the logical representation of the unit. This name can be up to 32 characters long and is stored in the project database only

Notes

This field contains a location to add notes about the unit which is stored in the project database only.

Status

This section contains information about the C-Bus network related functions located on the unit.

C-Bus Clock Active

This field indicates whether the C-Bus internal clock is enabled on this C-Bus unit. If activated, the indicator is lit. If not activated, the indicator is greyed out.

Voltage

This field contains the voltage level available to the unit.

PC_INTERFACE (NAC/SHAC/NAC2/AC2)

Global

This section allows you to check and update the C-Bus clock information.

C-Bus Clock

Select the check box to enable the resident C-Bus clock. Once you select the C-Bus Clock check box, the Save button is enabled.

 
 
 
 
 
 
 

Unit Identification

This section displays the fields for identification of the unit.

Unit Type

This field contains the unit type of the device.

Firmware Version

This field shows the version number of the C-Bus interface firmware which exists on the physical network or which has been assigned to a logical representation of the unit in the database.

NOTE: For PC_NAC/SHAC, the minimum firmware version to support is 5.5.00.

Catalogue Number

This field contains the catalog number related to the unit type.

Part Name

This field contains the part name which is stored in the unit hardware.

Unit Address

This field displays the unit address assigned to the device.

Serial Number

This field contains the serial number which exists on the physical network.

Tag Name

This field contains the name that user can give to the logical representation of the unit. This name can be up to 32 characters long and is stored in the project database only

Notes

This field contains a location to add notes about the unit which is stored in the project database only.

Status

This section contains information about the C-Bus network related functions located on the unit.

Voltage

This field contains the voltage level available to the unit.

Object List Manager

Object list manager allows you to work with assigned groups and levels of an application to the object list.

Controller Project List Manager window is displayed, which consists of the following:

Objects

Network

Displays network name of the selected object.

Application

Displays application name of the selected object.

Name

Displays name of the selected object.

Search

To search the existing objects in the object list, type the object name/application/network name in search bar.

Delete

Select the object list and click .

C-Bus Networks

C-Bus Network

All the available C-Bus networks are displayed in the drop-down.

Applications

All the available applications in the selected network are displayed in the drop-down.

NOTE: Applications of the selected network will be displayed.

Search

Depending on the type of application is selected groups, channels or devices can be searched using search bar.

Depending on the type of application is selected, groups, channels or devices are displayed.

Lighting Application

Group of the lighting application is displayed.

Address.

Displays address of the group/enable group.

Name.

Displays name of the group/enable group.

Enable

Group of the enable application is displayed.

Measurement Application

Channels of the measurement/error application are displayed.

Device ID.

Device ID to identify specific C-Bus unit fro measurement/error application.

Device Name.

Displays name of the device.

Error Application

Channel ID.

Object Id assigned to DALI Gateway (0–255).

Channel Name.

Specifies the name of the channel.

Emergency Exit Light

Devices of the emergency exit light application are displayed.

CDG Name.

Displays C-Bus DALI-2 Gateway name.

Line Name.

Displays DALI line name.

EEL Name.

Displays Emergency Exit Light application name.

Object ID.

Displays the Object ID of the device.

Test Group.

Displays the assigned test group.

  1. Click to add objects from C-Bus Network to the Object.

  2. Click to remove objects from Object.

  3. Click OK to save the object lists to project database.

    IMPORTANT:
    • The remote C-Bus network in the current project (connected via C-Bus bridge) allows up to a maximum of 19 networks along with local network (and 5 bridge networks deep max) allows to add objects in the object list section. Once the maximum limit is reached, the list of networks in the C-Bus Network will be disabled.

    • To use the disabled network, remove the objects in the object list.

    • Objects added to the list define the networks that will be used in the controller.

Transfer

The configurations in the SpaceLogic C-Bus Commission can be pushed to the C-Bus Controllers via push operation.

The created objects are pushed to the controller using Transfer button.

  1. Once the objects list are created, click Transfer. The C-Bus Controller Authentication window is displayed.

  2. Select the Interface type from drop-down.

    • Local TCP Connection

    • Remote TCP Connection

    • USB Connection

      NOTE: The IP address for Local, Remote and USB are fetched from the details configured in the IP layer.
    • Temporary TCP Connection

      For temporary connection, you need to enter additional IP address and HTTPS port details.

  3. Enter the password.

    NOTE: If you enter wrong password, Authentication Failed message is displayed.

  4. Click OK and re-enter the password.

  5. Click Login.

    The C-Bus controller Sync process window is displayed.

    The tag map and object informations are transferred to C-Bus Controllers.

    NOTE: Click Cancel to cancel the syncing.

    Click Yes.

    IMPORTANT: While transferring :
    • If there are any duplicates items identified (application, group or label name), C-Bus Controller Sync window is displayed indicating the duplicate items.

  6. Click Continue to resolve duplicate items.

    If any conflict items are identified, C-Bus Controller Sync window is displayed indicating the conflicts.

  7. Click Continue to resolve the conflict.

    On successful transfer, transfer completion message is displayed.

  8. Click OK to complete the transfer.

Retrieve

The configurations done in the controllers can be pulled from C-Bus Controller to the SpaceLogic C-Bus Commission using pull operation.

The created objects are pulled to the SpaceLogic C-Bus Commission using Retrieve button.

NOTE: When you extract any C-Bus device and try to configure controllers in parallel, the Retrieve button is disabled.

  1. Click Retrieve. C-Bus Controller Authentication window is displayed.

  2. Select the Interface type from drop-down.

    • Local TCP Connection

    • Remote TCP Connection

    • USB Connection

      NOTE: The IP address for Local, Remote and USB are fetched from the details configured in the IP layer.
    • Temporary TCP Connection

      For temporary connection, you need to enter additional IP address and HTTPS port details.

  3. Enter the password.

    NOTE: If you enter the wrong password, Authentication Failed message is displayed.

  4. Click OK and re-enter the password.

  5. Click Login. C-Bus controller Sync pop-up window is displayed.

    While retrieving (pull operation) data from C-Bus controllers, objects can be updated, deleted or added.

    NOTE:
    • To cancel the syncing, click Cancel.

      Click Yes.

    • An error message is displayed if the controller configuration is failed.

      Check the local and network IP address of the controller and re-login.

    IMPORTANT: While retrieving :
    • If any duplicates items are identified (application, group or label name), C-Bus Controller Sync window is displayed indicating the duplicate items

  6. Click Continue to resolve duplicate items.

    If any conflict items are identified, C-Bus Controller Sync window is displayed indicating the conflicts.

  7. Click Continue to resolve the conflict.

    On successful retrieve, completion message is displayed.

  8. Click OK to complete the retrieve.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.