Software Version 2.14.0

Sort Test Devices

Prerequisites: The Test Devices must already be added in the Devices section.

The existing devices in an application can be sorted.

  1. Select the device.

    NOTE:
    • A single device can be chosen by selecting the check box of the required group, whereas all devices can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one device, then hold down the SHIFT key and select on additional devices (grid) using the mouse.

    • For random multiple selection, select one device, then hold down the CTRL key and select the next device (grid) using the mouse.

  2. Click in the Devices section.

    The available sort methods are displayed.

  3. Select the appropriate sort method. The devices list will be sorted according to the selected sort method.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.