Software Version 2.14.0

Digital Dimmers

The SpaceLogic C-Bus Digital Dimmers are new-generation lighting control dimmers that helps to allow full customization for elegant control of dimmable LED lights and other light sources. The C-Bus dimmer is compatible with a range of load types.

  • Trailing edge for incandescent and capacitive input electronic transformer based LV lighting.

  • Leading edge for iron-core transformer based LV or neon lighting and other inductive loads.

Unit Types

  • DIMDD8 (5508D1D, 8 Channel 1A DIN Digital Dimmer with switchable C-Bus Power Supply)

  • DIMDD4 (5504D2D, 4 Channel 2A DIN Digital Dimmer with switchable C-Bus Power Supply)

  • DIMDH4 (5504DHD, 4 Channel High Power DIN Digital Dimmer with switchable C-Bus Power Supply)

To convert old dimmers to new dimmers, click here.

To upgrade Digital Dimmer firmware, click here.

To confirm channel dimming mode via live networks, click here.

To enable/disable Inbuilt C-Bus Power Supply function for the Digital Dimmers, click here.

WARNING
Dangerous voltages may be present on the output of dimmer channels even though the dimming level is set to zero.
Avoid the risk of electrical shock that could result in death or serious injury by disconnecting the unit from mains power before accessing the output terminals or any connected wiring. This condition is found on many dimming products.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The field information to configure SpaceLogic C-Bus Dimmers is as explained below:

Name

This field allows to modify the Dimmer device name.

Type

This field displays the default device type.

Applications

This section displays the lighting applications supported by the dimmers. Up to four lighting applications can be defined and then used throughout the configuration of the dimmers.

NOTE: Name, and Type are database properties only and not stored in device.

Channels

NOTE :

  • DIMDD8 will have 8 channels

  • DIMDD4 will have 4 channels

Group

This field allows to program group addresses associated with dimmer channels.

You can:

  • Select group address using drop-down list.

  • Modify group address using .

  • Add group address using .

  • Create a new group name which takes the next available address (it’s a fast commissioning option).

Dimming Mode

This field allows to select type of the Dimming Mode: Trailing Edge (TE) or Leading Edge (LE).

Channel Name

This field allows to define the channel name of the dimmer.

Channel Location

This field allows to define the channel location of the dimmer.

Advanced

Min Level

This field allows to set the minimum level in percentage.

Max Level

This field allows to set the maximum level in percentage.

Warn Before off Time

This field allows to set the warn before off time. By default, it is Not enabled.

Load Profile

Load profile feature allows to set the dimming channel to operate on specific load. By default, the inbuilt load profile is connected to the dimming mode selected.

Maximum of 4 custom profiles can be selected using drop-down list. Custom load profile can be modified using . For more details, click here

For more details on custom profile live testing, click here.

Dimming Curve

For more details, click here.

Power Recovery

This field allows to set the power recovery percentage. By default, it is Restore To Previous.

Power On Delay

This field allows to set the Power On Delay in hours: seconds format.

Logic

Type

This field allows to select the type of the logic group.

Logic Group

This field allows to program logic group addresses associated with dimmer channels.

You can:

  • Select group address using drop-down list.

  • Modify group address using 

  • Add group address using .

  • Have maximum 4 logic groups.

Warn Before off

This section indicates warning off before the group address is turned off (1–15 minutes) based on the timings set.

Warn Before off Enable Group

It also allows to create a new group name which takes the next available address.

In this section, you can :

  • Create a enable group using .

  • Modify existing group using .

By default, it is unused. If enable group is created, Restore To Previous is enabled.

By typing new name in <unused> space allows you to create a new group name which takes the next available address.

Restore To Previous

If Restore To Previous is unchecked, recovery level is enabled to set. By default, Restore To Previous is checked.

Recovery Level

Recovery level percentage can be from 0 –100%

Remote On/Off

This field allows to choose the combinations of Remote On and Off for each individual channels.

NOTE :

  • DIMDD8 will have 8 channels

  • DIMDD4 will have 4 channels

Error Reporting

This section displays the fields for error reporting

Firmware Version

Applicable for firmware version below 1.1.0

Applicable for firmware version above 1.1.0

Device ID

This field displays the unit address of the device.

NOTE: The Device ID is for the entire device and is as same for Measurement section.

This field displays the unit address of the device.

NOTE: The Device ID is for the entire device and is as same for Measurement.

When you assign a Device ID, and then if you set the Device ID to Not Assigned, then all properties in both the Error Reporting and Measurement section are reverted to their default settings and disabled (grey out state).

Mouse over on the Device ID info icon to view the tooltip message.

Mode Control Group

This field allows to add an enable group (0–254).

If you assign a group, Restore To Previous field is displayed and Regular Reporting Interval drop-down is enabled.

If you uncheck Restore To Previous check box, Regular Reporting field will be enabled.

If you check Restore To Previous check box, Regular Reporting will be disabled.

Regular Reporting

This field configures the Error Reporting mode of the Dimmers into one of three modes:

  • Triggered only: Errors are reported only when triggered by the assigned Trigger Group.

  • Always ON, most recent only: The most recent errors are reported automatically at a regular time interval (time set by the Regular Report Interval field).

  • Always ON, most recent and most severe: The most recent and most severe (or latched) errors are reported automatically at a regular time interval (time set by the Regular Report Interval field).

This field configures the Error Reporting mode of the Dimmers into one of the modes:

  • Disabled (Triggered only)

  • All Errors, Most Recent only:

  • All Errors, Most Recent and Most Severe (Mode 2)

  • Minimum Errors, Most Recent only (Mode 3)

  • Minimum Errors, Most Recent and Most Severe (Mode 4)

All the modes can be set with the regular reporting interval set to No regular reports, which allows live reporting of errors without the regular reports.

Mouse over on the Regular Reporting info icon to view the tooltip message.

Restore to Previous

If selected, this field restores the data on power failure.

When you click Save with the below conditions:

  • Mode Control Group — Assigned

  • Restore to Previous — Checked

  • Regular Reporting — Disabled state

The Regular Reporting displays the last saved value.

Mouse over on the Restore to Previous info icon to view the tooltip message.

Regular Reporting Interval

This field is used to select the time interval period between the completion of a regular report and beginning of the next report in Always On, Most recent only and Always On, Most recent and most severe modes. By default, the interval is 30 minutes.

Regular reporting interval is enabled for Trigger only mode.

Trigger Group

This field contains a Trigger Group to trigger an error reporting event for any of the three error reporting modes. When a Trigger group is created, Resend Action Selector and Acknowledge Action selector are displayed.

The Resend Action Selector is set to send all errors and Acknowledge Action selector is set to acknowledge all errors.

Destination Network

This field contains the destination C-Bus network to which the Dimmers routes the error reporting messages. This allows the error messages to be sent to a remote C-Bus network for central monitoring if it’s not the local network.

Mouse over on the Destination Network info icon to view the tooltip message.

Application Items

The Property Editor displays the Application Items property only when you load a project C-Bus Dimmer device. When you load a live network C-Bus Dimmer device, the Property Editor hides this property because you can create application data only for a project device.

Mouse over on the Application Items info icon to view the tooltip message.

For more info on bulk creation of application data for dimmers, click here.

Advanced

C-Bus Voltage Warning Set Threshold

  • By default, Disabled is selected

  • The value selected must be less than the C-Bus Voltage Warning Clear Threshold value selected.

  • If the C-Bus Voltage Warning Clear Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Warning Clear Threshold value to (current C-Bus Voltage Warning Set Threshold value + 1 V).

Mouse over on the C-Bus Voltage Warning Set Threshold info icon to view the tooltip message.

C-Bus Voltage Warning Clear Threshold

  • By default, Disabled is selected.

  • The value selected must be greater than the C-Bus Voltage Warning Set Threshold value selected.

  • If the C-Bus Voltage Warning Set Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Warning Set Threshold value to (current C-Bus Voltage Warning Clear Threshold value - 1 V).

Mouse over on the C-Bus Voltage Warning Clear Threshold info icon to view the tooltip message.

C-Bus Voltage Critical Set Threshold

  • By default, Disabled is selected.

  • The value selected must be less than the C-Bus Voltage Critical Clear Threshold value selected.

  • If the C-Bus Voltage Critical Clear Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Critical Clear Threshold value to (current C-Bus Voltage Critical Set Threshold value + 1 V).

  • If the C-Bus Voltage Warning Set Threshold has a value set (other than Disabled), then the value selected must be less than (current C-Bus Voltage Warning Set Threshold value).

Mouse over on the C-Bus Voltage Critical Set Threshold info icon to view the tooltip message.

C-Bus Voltage Critical Clear Threshold

  • By default, Disabled is selected.

  • The value selected must be greater than the C-Bus Voltage Critical Set Threshold value selected.

  • If the C-Bus Voltage Critical Set Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Critical Set Threshold value to (current C-Bus Voltage Critical Clear Threshold value - 1 V).

Mouse over on the C-Bus Voltage Critical Clear Threshold info icon to view the tooltip message.

C-Bus Power Supply Warning Set Threshold

  • By default, Disabled is selected.

  • The value selected must be greater than the C-Bus Power Supply Warning Clear Threshold value selected.

  • If the C-Bus Power Supply Warning Clear Threshold is Disabled, then setting a value here will also set the C-Bus Power Supply Warning Clear Threshold value to (current C-Bus Power Supply Warning Set Threshold value - 10 mA)

Mouse over on the C-Bus Power Supply Warning Set Threshold info icon to view the tooltip message.

C-Bus Power Supply Warning Clear Threshold

  • By default, Disabled is selected.

  • The value selected must be less than the C-Bus Power Supply Warning Set Threshold value selected.

  • If the C-Bus Power Supply Warning Set Threshold is Disabled, then setting a value here will also set the C-Bus Power Supply Warning Set Threshold value to (current C-Bus Power Supply Warning Clear Threshold value + 10 mA).

Mouse over on the C-Bus Power Supply Warning Clear Threshold info icon to view the tooltip message.

Unit Over Temperature Set Threshold

This field is a combo box which is by default set to 70° C .

The Unit Over Temperature Set Threshold property increments by 1° C with a range of 1° C - 80° C.

Mouse over on the Unit Over Temperature Set Threshold info icon to view the tooltip message.

Unit Over Temperature Clear Threshold

This field is a combo box which is by default set to 65° C .

The Unit Over Temperature Clear Threshold property increments by 1° C with a range of 0° C - 79° C.

Mouse over on the Unit Over Temperature Clear Threshold info icon to view the tooltip message.

 

Firmware Version

Applicable for firmware version below 1.1.0

Applicable for firmware version above 1.1.0

Measurement

Device ID

This field displays the unit address of the device

NOTE: The Device ID is for the entire device and is as same for Error Reporting section.

This field displays the unit address of the device.

NOTE: The Device ID is for the entire device and is as same for Error Reporting section.

When you assign a Device ID, and then if you set the Device ID to Not Assigned, then all properties in both the Error Reporting and Measurement section are reverted to their default settings and disabled (grey out state).

Mouse over on the Device ID info icon to view the tooltip message.

Send Trigger Group

This field contains a trigger group to request the Dimmers to send its stored measurement data.

Mouse over on the Send Trigger Group info icon to view the tooltip message.

Clear Trigger Group

This field contains a trigger group to clear the stored measurement data in the dimmers.

Mouse over on the Clear Trigger Group info icon to view the tooltip message.

Regular Broadcast Interval

NA

Disabled by default. Can set the intervals between 1 min to 4 hours.

Regular Broadcast Option

NA

All

Enabled by default

Lamp Hours

Selected and Disabled by default

Channel Temperature

Selected and Disabled by default

Power Supply Current

Selected and Disabled by default

C-Bus Voltage

Selected and Disabled by default

Unit temperature

Selected and Disabled by default

NOTE: Deselecting all will enable each of the individual check box options.
Destination Network

This field contains the destination C-Bus network to which the dimmer routes measurement application messages.

Mouse over on the Destination Network info icon to view the tooltip message.

The action selector for trigger groups is as explained below:

Virtual Channel Number

Property

Units

Reset

Notes

0 – 15

Lamp Running Time

Hours

Yes

NA

16 – 31

Channel Voltage

Volts

No

Units with power metering only

32 – 47

Channel Current

Amperes

No

48 – 63

Channel Power

Watts

No

64 – 79

Channel Energy

Watt-hours

Yes

80 – 95

Channel Lifetime Energy

Watt-hours

No

128 – 143

Channel Temperature

Celsius

No

Dimmers only

252

C-Bus Power Supply Output Current

Amperes

No

NA

253

C-Bus Voltage

Volts

No

NA

254

Unit Temperature

Celsius

NA

NA

Measurement Application supports various operational parameters for triggered request.

Measurement Request Trigger Group defines the Trigger Group for the request. A trigger's Action Selector determines which measured parameter is requested.

NOTE: Action Selector 0xFF requests all measurements (in which they are sent 2 at a time with an interval of 2 seconds). Other Action Selector values can be used to request individual measured properties corresponding to the virtual channel number as per the above table.

The DEVICE ID for the Measurements is defined by the Device ID parameter, the same Device ID is used for Error Reporting. The Device ID will be unique per network to differentiate measurements from different devices. The devices monitoring the Measurement messages should keep track of the source network to differentiate if Device IDs are reused across multiple C-Bus networks.

If the Device ID parameter is left at its default value of 0xFF then the Unit Address is used as the Device ID in the Measurement Application messages, which ensures uniqueness. However, if the device is readdressed then any monitoring devices will also needs to be updated to match the new Device ID (It is recommended to leave the Device ID as the default value).

Logic Groups

Dimmers can have maximum 4 logic groups each group having respective channels (8 or 4)

Group

This section will allow to create a enable group using and modify existing group using .

By default, it is unused. If enable group is created, Restore To Previous is enabled.

Power Recovery

This field allows to set the power recovery percentage. By default, it is Restore to previous.

Channel

NOTE :

  • DIMDD8 will have 8 channels

  • DIMDD4 will have 4 channels

Global

This section displays the project properties set by the user at the time of creation of the project.

C-Bus Clock

If checked, allows you to enable the C-Bus clock for the dimmers.

Disable Local Toggle

If checked, disables the local toggle.

Network Hardware Burden

If checked, the physical hardware burden is plugged into the device.

By default, it is unchecked.

Inbuilt C-Bus Power Supply

If checked, the power supply is enabled/active.

By default, it is unchecked.

Disable Dimmer Mode Change

If checked, disables the dimmer mode change.

Disable Power Supply Toggle

If checked, disables the power supply toggle.

Disable C-Bus Priority

If checked, disables the C-Bus priority.

Disable Clock Generator Toggle

If checked, disables the clock generator toggle.

Unit Identification

This section display the fields for identification of the unit.

Unit Type

This field contains the unit type and unit description of the device.

Catalog Number

This field contains the catalog number related to the unit type.

Firmware Version

This field shows the version number of the C-Bus interface firmware which exists on the physical network or which has been assigned to a logical representation of the unit in the database.

Part Name

This field contains the part name which is stored in the unit hardware, which can be modified.

Unit Address

This field displays the unit address assigned to the device.

Serial Number

This field contains the serial number which exists on the physical network.

Tag Name

This field contains the name that user can give to the logical representation of the unit. This name can be up to 32 characters long and is stored in the project database only.

Notes

This field contains a location to add notes about the unit which is stored in the project database only.

Status

The Status section contains information about the C-Bus network related functions located on the unit.

Device Status

This section displays the details of hardware.

Hardware Version

This field displays the hardware version of the device.

Firmware Version

This field displays the firmware version of the device.

C-Bus Clock Active

This field indicates whether the C-Bus internal clock is currently enabled on the Dimmers on the network.

C-Bus Voltage (V)

This field displays the C-Bus voltage of the device.

Inbuilt C-Bus Power Supply Active

This field displays whether the Inbuilt C-Bus Power Supply Active is On or Off.

Power Supply Load

This field displays the load of the power supply (mA).

Power Supply Output Voltage

This field displays the power supply output voltage (mV) of the device.

Load Power

This field displays the load power (mW) of the device.

Unit Temperature

This field displays the unit temperature (°C)of the device.

Channel Status

Each channel will have these channel status.

NOTE :

  • DIMDD8 will have 8 channels

  • DIMDD4 will have 4 channels

Load Compatibility

This field displays the status of load incompatibility (Yes/No).

Dimming Mode

This field displays type of the dimming mode.

Offline

This field displays the status of the device (Yes/No).

Dimming Mode Error

This field displays the status of dimming mode error (Yes/No).

Temperature Wind Back

This field displays the status of temperature wind back (Yes/No).

Temperature Shut Down

This field displays the status of temperature shut down (Yes/No).

Over Current

This field displays the status of over current (Yes/No).

Operating Temperature

This field displays the value of the temperature.

Mains Frequency

This field displays the value of the mains frequency.

Once configuring dimmers is completed save the changes.

Load Profile

By adjusting settings within each dimmer channel, a Load Profile tailors dimming behavior for better end-to-end performance.

Inbuilt Load Profiles and the Inbuilt Dimming Curve have the pre configured settings which cannot be modified. If the acceptable results cannot be utilized with the load being used, the settings are customized and applied to a dimmer channel.

A Custom file can also be saved and used within other channels of the dimmer and also shared across other compatible dimmer devices.

Default Dimmer Channel Profile is selected to be the most universal. There are 4 user-configurable dimmer channel profiles. Each channel can be assigned to any one of these 5 profiles. In each case there is a improvement for the light source behavior during dimming, the load profile can be adjusted by the SpaceLogic C- Bus Commission Software.

NOTE: The Load Brand, Load Model, Load Quantity, Custom Notes, Load Type and Mains Frequency fields are saved as project settings only. Furthermore, the Load Type and Mains Frequency selections determine the values presented in the Custom Load Profile section.

The SpaceLogic C-Bus Commission software allows:

  • The customizing of the load profiles per channel.

  • 4 user configurable profile per channel/device.

  • Saving and sharing of endless load profiles for future project uses.

  • Different load types:

    • LED Lighting (TE Dimmable)

    • LED Lighting (LE Dimmable)

    • Electronic Transformer (TE Dimmable)

    • Electronic Transformer (LE Dimmable)

    • Incandescent Lighting (TE Preferred)

    • Incandescent Lighting (LE)

    • Iron Core Transformer (LE)

    • Sweep Fan (LE)

    • Exhaust Fan (LE)

    • Other (LE)

    • Other (TE)

To create a customized load profile:

  1. Under Advanced section of Channels, select any Custom Profile option from Load Profile drop-down.

  2. Click .

    Custom Load Profile and Dimming Curve window is displayed. The load profile customizing is done in Configuration tab.

    For 50 Hz

    For 60 Hz

    NOTE: The Custom Load Profile parameter values varies depending on the load type selected.

    • The lower limit for the Soft Turn On property is calculated dynamically. However the lower limit value is no less than 0.01.

    • The lower limit for the Soft Turn Off property is calculated dynamically. However the lower limit value is no less than 0.01.

    • The lower limit for the Kickstart Brightness is based on Minimum Brightness + 10.

    • The lower limit for the Kickstart Turn On property is calculated dynamically. However the lower limit value is no less than 0.01.

    • Selecting a Load Type will load specific values based on the selection of the Mains Frequency property.

    IMPORTANT: When deploying a DIMDD8 / DIMDD4 dimmer, the dimming mode of each channel of the dimmer device loaded into the Property Editor are compared to the live dimmer device. If there is a conflict in the dimming mode of a channel :

    A Channel Dimming Mode Conflict window is displayed prior to deployment.

    • Click Yes to resolve the conflict and deploy.

    • Click No to cancel the deployment.

  3. SpaceLogic C-Bus Commission enables saving, uploading or sharing of load profile files which includes the following :

    • Load Brand

    • Load Model

    • Load Quantity

    • Custom Notes associated with the load

    • Load Type

    • Read-only dimming mode

    • Mains Frequency

    Dimming setting includes the following:

  4. To edit the preset values, click on the value and type new value within the range which is mentioned next to the parameter.

  5. Click to reset the parameter values.


Minimum Brightness: Sets the level where the load operates or is visibly On.

Maximum Brightness: Sets the level where the load exhibits no further change in brightness or output.

Soft Turn On: Sets the role of change for Instant Ramps. The value is the time taken to transit from Off to Maximum Brightness. This value can also affect the timing of C-Bus Ramps between levels and the output of a dimming curve, which is set to 1 second or less.

Soft Turn Off: Sets the role of change for Instant Ramps. The value is the time taken to transit from Off to ON.

Kickstart Duration: When enabled, sets the duration to maintain the Kickstart Brightness level before recovering to a lower level if set.

Kickstart Brightness: When enabled, sets the dimmer Kickstart Minimum Brightness level before when transition from Off to On (at any level).

Kickstart Turn On: When enabled, sets the time in which the Kickstart Brightness level is applied to the load. A value of 10 ms is a Fast or Hard Start (same as a switch). This value is recommended to be set to Fast between 0.010 ton 0.100 seconds.

Kickstart Recovery: When enabled, sets the time taken at the end of the Kickstart duration to transition from the Kickstart Brightness level to the currently set level of the load.

If the set level is less than the Kickstart Brightness level, this value is set to Slow to achieve a smooth unnoticeable transition at the end of the kickstart.

To reset both Load Profile and Dimming Curve set values, click Reset All.

Enter the required information in Load Brand, Load Model, Load Quantity and Profile notes and click OK.

The custom load profile settings created can be saved and used for other dimmer channels and dimmer devices by exporting the settings using Save To File. The Save to file is enabled once there is a change in the settings.

The exported custom load profile can be reloaded to use for other dimmers using Read From File . This will open the folder consisting of JSON files in the path Assets > Load Profile and Dimming Curve Files.

Select the file and click Open.

Custom Profile Live Testing

Custom Profile Live Testing allows you to quickly identify and define the minimum and maximum conduction values for a dimmer channel. It uses a direct connection to the dimmer and provides live control of the connected load, without repetitive deployment including:

  • Maximize dimming range of connected lights.

  • Mask erratic behavior of lights at low brightness levels.

  • Mask little/no change in response of lights at high C-Bus control levels.

  • Define attributes from live testing rather than experimenting or guessing values to try.

    NOTE: The maximum conduction value has been changed to 9000 for High-powered dimmer (DIMDH4) and to 9500 for other dimmers.

To perform live testing on the dimmer:

  1. In the PROPERTIES window, select any custom profile from the Load Profile drop-down and click .

    Custom Load Profile and Dimming Curve window is displayed.

  2. You can perform live testing in the Testing section. The Testing tab is disabled initially and becomes enabled when the following conditions are met:

    • The C-Bus Network must be opened and scanned.

    • If the dimmer is invoked from project, dimmer must be partial or fully matched.

    • A group address must be set or configured to the channel.

      The Testing tab displays the below properties of the dimmer:

      • Dimmer Device Name.

      • Dimmer Channel Name.

      • Current configured Load Profile for the channel.

      • Current configured Dimming Curve for the channel.

      • Current configured Dimming Mode for the channel.

      • Current configured Mains Frequency for the channel.

  3. Click to start the testing.

    NOTE: The testing operation places the current dimmer channel into test mode, allowing you to explore, test and confirm its dimming capability with the connected load.
  4. Once the testing starts, the process takes place in three steps.

    Step 1:

    1. Set the lowest acceptable brightness level and click Set Value to set the value.

      NOTE: Until you set the value and click Set Value, the Turn On and Turn Off buttons will be disabled.
    2. Click Turn On to test the turn on behavior at that level.

    3. Click Turn Off to turn off the test at that level.

    4. Click Step 2 to test the maximum brightness.

    Step 2:

    1. Set the highest acceptable brightness level.

    2. Click Step 3 to test the dimming response.

    Step 3:

    1. Choose the ramp rate response between the Minimum and Maximum Brightness limits with the load currently connected, to test and observe the dimming behavior within the range defined in Step 1 and Step 2.

      The ramp rate ranges are instant, 4 secs, 8 secs, 12 secs, 20 secs, 30 secs.

    2. Click Save.

    NOTE: If a validation error occurs, the step arrows and labels are disabled.

Dimming Curve

A Dimming Curve refers to a translation between input level and output level. A Dimming Curve adjusts the rate of the change of the brightness level of a dimmer channel as the C-Bus group (level) is ramped. The default dimming curve is linear.

To create a customized Dimming Curve:

  1. In Advanced section of channels, select Custom Curve from the Dimming Curve drop-down.

  2. Click .

    Custom Load Profile And Dimming Curve window is displayed.

  3. To add new point on chart, right click on the chart and select Add.

  4. To change the added point, hold and drag the point to set new channel and control range value.

    Once settings are completed mention curve notes and confirm OK.

    The chart in below image represents mapping between load profile and C-Bus control range.

    The custom dimming curve settings created can be saved and used for other dimmer channels and dimmer devices by exporting the settings using Save To File. The Save to file is enabled once there is a change in the settings.

  5. Click to reset the setting values.

    The exported custom dimming curve can be reloaded to use for other dimmers using Read From File . This will open the folder consisting of json files in the path Assets > Load Profile and Dimming Curve Files.

  6. Select the file and click open.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.