Software Version 2.14.0

Deployment Queue

The Deployment Queue displays the status of devices that are being extracted to Devices in Project and configured devices that are being deployed to the hardware. The devices can be identified in the physical device configuration.

Prerequisites: The network must already be created in project. Devices in Project must have been fully matched with Network devices.

The Deployment Queue allows reconciliation of the Devices in the Project and the network. The reconciled devices can then be deployed to the network. This Queue also allows searching for a device, by entering the device name, part number or description fully or partly in the search bar.

To Deploy any device once the configuring is completed, Save the settings and check Deploy to Network. or after saving the settings click on Devices in Project section.

To remove the Deployed devices based on Waiting, Failed, Completed Click drop-down.

The Deployment Queue consists of following tabs:

  • Active

    This tab consists of devices that are currently active in deployment process.

  • Completed

    This tab consists of devices that has finished the activity in deployment queue..

Field

Meaning

Activity

This field displays the activity of the unit device, whether the Unit device is being extracted or being deployed.

Added

Displays The time unit device was added to deployment queue.

Duration

Displays the time taken for the activity

Message

Displays the message whether the activity was failed, successful or Done.

Target Network

Displays the network through which the unit device was deployed.

IMPORTANT: When Deployment activities are in progress performing following actions are not possible:
  • Closing a network

  • Switching between the projects

  • Closing a project

  • Exiting an application or software

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.