Software Version 2.14.0

Add Measurement Data

Prerequisites: The Measurement application must already be created in a network.
  1. Click Applications drop-down in the EXPLORER window.
  2. Click Measurement
  3. Click

    Step result: A Measurement detail is added.

    NOTE:
    • A Measurement detail can be deleted during creation/adding itself using “x” as shown below:

  4. The Channel and Device name of the measurement data can be modified. Double-click on the channel/device name, edit the device name to match your device and channel name to match the channel that is been monitored on the device, then click enter (or on the empty space of the section) to update the change.
    NOTE: Device ID and Device name combination is unique. A Device ID can only belong to the same device name. Modifying the Device Name for One Device ID will update for all the Channels with same Device ID. A Device ID is unique on the network. But there can be multiple device channels on the same device.
TIP: A single Device ID can have multiple Channel ID. The procedure to add multiple measurement data for the same Device ID is as demonstrated below:
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.