Software Version 2.14.0

Delete Trigger Groups

The delete function allows you to delete one or more group addresses from a Trigger application.
Prerequisites: The trigger group address must already be created in the Trigger application.
  1. Click Applications > Trigger.
  2. Select the Trigger Group check box to be deleted in the Trigger Groups section.
    NOTE:
    • A single trigger group can be chosen by selecting the check box of the required group, whereas all trigger groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one trigger group, then hold down the SHIFT key and select on additional groups (grids) using the mouse.

    • For random multiple selection, select one trigger group, then hold down the CTRL key and select the next trigger groups (grids) using the mouse.

    • The option will be disabled, if a trigger group is not selected.

  3. Click in the Trigger Groups section. A Confirmation pop-up is displayed.
  4. Click Yes to delete the trigger group.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.