Software Version 2.14.0

Paste Enable Groups

The Enable application Group Addresses copied from one network are pasted either into another Enable application in same network or in a different network, or in different project.
Prerequisites: The Enable Group Address must be copied from an application to another network or to the same network.
NOTE: The Enable application Group Address copied from one network must be pasted only into the Enable application on another network.
  1. Select the Enable application of the network to be pasted in
  2. Click in the Enable Group section
    NOTE: The process to Paste the Enable Groups from excel is similar to as demonstrated in lighting application, click here
IMPORTANT: Paste conflict occurs when already existing Enable group address and group name are been pasted.

The process to Resolve conflict is similar to as demonstrated in lighting application, click here

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.