Software Version 2.14.0

Media Transport Application

The Media Transport Control application is designed to transmit control signals for audio and video equipment used with C-Bus units.

Media Transport application is created using an reserved application number 192.

SpaceLogic C-Bus units which support audio application are:

  • CD and DVD recorders and players

  • Audio tuners

  • Personal video recorders (PVRs)

  • Media centres

  • MP3 streamers

These C-Bus units has a C-Bus interface to be controlled by Media Transport commands or have a converter which translates Media Transport commands into a form which is understood by C-Bus units.

The software packages that supports to handle Media Transport is C-Bus Ripple® audio streaming software.

The procedure to create a media application is as demonstrated below:

NOTE: To resolve the paste conflict of an application click here

Operations performed in Media application

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.