Software Version 2.14.0

Edit Values

Prerequisites: The Values must already be existing in the selected Enable group of Enable application.

  1. Double-click on the value name that has to be edited.

    Step result: Edit Value dialog box is displayed.
  2. Edit the Value name and click OK.

    NOTE: Special characters except /,”,# and maximum of 32 characters in the Values name are valid.

    Step result: The Value name is updated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.