Software Version 2.14.0

Support Units

C-Bus units which provide support for the C-Bus network are generally known as support units. Some support units are responsible for linking a C-Bus network to another network or other system or protocol. They include bridges to connect C-Bus networks to one another, DALI gateways to connect to DALI networks, and interface units to connect to PCs, laptops as well as third party control devices. Other support units include: Telephony interfaces, IR transmitters, and C-Bus power supplies.

These units physically link a C-Bus network to another network or other system or protocol. They include C-Bus bridges, which link two wired networks, as well as wired to wireless gateways to connect to C-Bus wired networks.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.