Software Version 2.14.0

C-Bus Settings

The operations that can be performed in the General Settings section are as follows:

Application Log

The Application Log allows the user to display group activity on the physical network. By default, the application log is toggled ON.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.