Software Version 2.14.0

Paste Trigger Groups

The Trigger application Group Addresses copied from one network are pasted either into another Trigger application in same network or in a different network.
Prerequisites: The Trigger Group Address must be already copied from an application.

NOTE: The Trigger application Group Address copied from one network must be pasted only into the trigger application on another network.
  1. Select the Trigger Groups in the Trigger application of the network to be pasted in.
  2. Click in the Trigger Group section.
    NOTE: The process to Paste the Trigger Groups from excel is similar to as demonstrated in lighting application, click here
IMPORTANT: Paste conflict occurs when already existing trigger group address and group name are been pasted in trigger application of another network.

The process to Resolve conflict is similar to as demonstrated in lighting application, click here

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.