Software Version 2.14.0

Overview of Project Space

The displays the different windows in the SpaceLogic C-Bus Commissioning software, which consists of:

Windows Description

EXPLORER

This window allows to view and manage all the networks created in the current project.

LIBRARY

This window allows to view the device catalogue details and relevant functions.

WORKSPACE

This window is the main area of display for project information which consists list of devices in the projects database and list of devices in the network.

PROPERTIES

This window allows to view the applicable properties of selected device in a single editor window.

DEPLOYMENT QUEUE

This window displays the process of devices being transferred to Devices in Project and getting deployed to Network devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.