Software Version 2.14.0

Safety Precautions

CAUTION
hazard of incorrect information
  • Do not incorrectly configure the software, as this can lead to incorrect reports and/or data results.
  • Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.
  • Do not rely solely on the software's messages and information for maintenance or service decisions.
  • Consider the implications of unanticipated transmission delays or failures of communications links.
Failure to follow these instructions can result in injury or equipment damage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.