Software Version 2.14.0

Add Groups

Prerequisites: The network must already be created in a project.
  1. Select a network from the Explorer window.
  2. Click Applications drop-down
  3. Select Lighting
    Step result: Respective Groups and levels section of Lighting is displayed in the Workspace window.
  4. Click in the Groups section.
  5. Choose address

    Step result: A Group is created.

    TIP: Multiple groups can be created at a time as demonstrated below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.