Software Version 2.14.0

Add Error Object

Prerequisites: The Error application must already be created in a network.
  1. Click Applications drop-down in the Explorer window
  2. Click Error
  3. Click

    NOTE:
    • The error object can be deleted during creation/adding itself using “x” as shown below:

    • The Channel and Device name of the error object can be modified. Double-click on the channel/device name, edit the device name to match your device and channel name to match the channel that is been monitored on the device, then click enter (or on the empty space of the section) to update the change

    • Warning dialog box is displayed while attempting to use an reserved channel name

    • Invalid Input message is displayed when attempting to use the channel name which is already belonging to a reserved channel

    The field informations of error application is as explained below:

    Field

    Meaning

    Device ID

    Unique Device ID is a reference to identify a specific C-Bus unit for error reporting purposes. The error Device ID drop down list allows the ability to select a value from 0- 254

    Device Name

    Specifies the name of the device

    Device Type

    Specifies the type of the device

    Channel ID

    Object Id assigned to the device

    IMPORTANT: Reserved channel Id’s have default channel names:
    • Channel Id 254: “Unit Error”

    • Channel Id 253: “Line B Error”

    • Channel Id 252: “Line A Error”

    • Channel Id 251: “Channel Aggregate Error”

    Channel Name

    Specifies the name of the channel

    NOTE: The channel names of reserved channel Id’s cannot be modified.

    Error Code

    Generated error code

    Error Status

    Description of the error status

    Action

    Action to be performed based on error:

    ACK: Acknowledge the error object

    Clear: Clears the error object

    Different Devices have an Channel ID references as explained below:

    DALI 2 Gateway

    0-63 DALI line A Object ID’s

    63-127 DALI line B Object ID's

    Dimmers

    8 Channel - 0-7

    4 Channel - 0-3

    NOTE: Each channel Id represents the respective Channel
    NOTE:
    • While adding new device, the device type can be selected using drop-down option

    • Click Ack, to acknowledge the particular error

    • Click Clear, to clear the error code and status

    Step result: A Error object is added.

    IMPORTANT: Error code and error message for each device are read from the live network devices and will be displayed on error table against corresponding device and channel ID.

TIP: A single Device ID can have multiple Channel ID. The procedure to add multiple error object for the same Device ID is as demonstrated below (maximum of 255 devices can be added at one go):

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.