Software Version 2.14.0

Edit Groups

Prerequisites: Make sure you have selected Lighting application and group has been created.
  1. Double-click on the group name that has to be edited/renamed
    Step result: Edit Group Dialog box is displayed.
  2. Edit the Group name and click OK
    NOTE: Special characters except /,”,# and maximum of 32 characters in the group name is acceptable.
    Step result: The Group name is updated.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.