Software Version 2.14.0

Overview

Introduction to SpaceLogic C-Bus

SpaceLogic C-Bus is a lighting and building automation system in a commercial or residential building. It allows the user to manage lights, shutters, temperature, security and energy usage.

In this document, the term 'software' refers to the "SpaceLogic C-Bus Commission" software.

C-Bus Architecture

The C-Bus architecture includes some important components:

  • A messaging protocol that connects building automation applications

  • A large set of units which can send and receive one or more building automation applications

  • Addressing protocols that identify units, building automation applications, and networks uniquely

  • A set of bridges and gateways which allow the transmission of C-Bus messages across C-Bus networks

  • A peripheral interface unit (PCI) which transmits configuration information between SpaceLogic C-Bus commission, which is the C-Bus network configuration utility, and C-Bus networks

C-Bus system Architecture for Commercial Buildings


Small Commercial Buildings


Large Commercial Buildings

C-Bus system Architecture for Residential Buildings


Single Dwelling Residential Buildings


Multi-Dwelling Residential Buildings

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.