Software Version 2.14.0

Delete Enable Group

The delete group allows you to delete one or more group addresses from a Enable application.
Prerequisites: The enable group address must already be created in the Enable application
  1. Click Application > Enable.
  2. Select the Enable Group check box to be deleted in the Enable Groups section.
    NOTE:
    • A single enable group can be chosen by selecting the check box of the required group, whereas all enable groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one enable group, then hold down the SHIFT key and select on additional groups (grid) using the mouse.

    • For random multiple selection, select one enable group, then hold down the CTRL key and select the next enable groups (grid) using the mouse.

    • The option will be disabled, if a enable group is not selected.

  3. Click in the Enable Groups section. A Confirmation pop-up is displayed.
  4. Click Yes to delete the enable group.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.