Software Version 2.14.0

Enable Application

When a network is created in project, the Enable application is created by default with an application number 203.

The Enable application is viewed similar to lighting application, click here

For more details, click:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.