Software Version 2.14.0

Lighting Application

The lighting applications are responsible for controlling electrical loads for a wide range of automation operations.

The Lighting application contains functions for editing the application and related lighting compatible groups. Each of the Group and Level entries contains information in the fields.

When a network is created in project, the Lighting application is created by default with an application number 56 and ranges from 48 to 127 (applicable while creating new lighting application).

For more details, click:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.