Software Version 2.14.0

Projects Management

The management of projects consists of operations that can be performed on projects individually in the software.

The projects tool bar in the project home screen include project name.

Operations performed on project screen.

Icons Operation

Close the current project, see Close project

Windows Drop-down menu, see Overview of Project space

Operations performed on projects dashboard:

Create a Project

Prerequisites: The SpaceLogic C-Bus Software must be opened.

  1. Click in the Projects dashboard.

    or,

    Click > to create a new project.

    The New Project pop-up is displayed.

  2. Enter the required information about the project and click Create.

    A new project is created.

Switch Projects

SpaceLogic C-Bus Commission software allows you to switch between the projects.

Prerequisites: More than one project must already be created.

  1. Click in the projects dashboard.

  2. Click of the individual project to be switched.

  3. Select Open.

    Confirmation pop-up appears.

  4. Click Yes to switch the projects.

    Step result: Your selected project is opened.

IMPORTANT:
  • Trying to switch a project while deployment activities are in progress is not possible.

  • Trying to switch a project while scanning is in progress is not possible.

Open an Existing Project

Pre-requisites: The project must already be created.

  1. Click in the projects dashboard.

  2. Click of the individual project to be opened.

  3. Select Open.

  4. Click Yes to open the existing project.

Edit a Project

SpaceLogic C-Bus Commission software allows you to edit an existing project so that you can correct or update the information to keep it accurate and relevant.

Pre-requisites: The project must already be created.

  1. Click in the Projects dashboard.

  2. Click and select Edit Project.

    or,

    Right-click on the project in the Projects dashboard.

  3. Select Edit Project to open the Edit Project pop-up.

  4. Modify the project information.

    • In Project Name field, rename the project name. Project name should be unique (between 1-8 characters, uppercase ASCII letters and numbers, and underscores).

    • In Description field, enter the description.

    • In Customer Contact field, modify if required.

    • In Address field, provide the address details.

    • In City field, enter the city name.

    • In State field, enter the state name.

    • In Country field, when you start to type in, the drop-down list automatically filters to display only matching results. The selection updates dynamically based on the input.

      • By default, the Country field is populated using the personal computer’s windows regional settings to reflect your local country.

    • In Postcode field, enter the postcode.

      NOTE: The Address, City, State and Pincode fields allows up to 254 characters. Special characters such as #, &, and / are not allowed.
  5. Click Save to update the changes.

    Below are the error scenarios:

    • An error pop-up appears when you hover on the icon, if the project name already exists.

    • An error pop-up appears when you hover on the icon, if the project is already opened in C-Gate. 

      NOTE: Save button will be disabled.

Search a Project

Pre-requisites: The project must already be created.

SpaceLogic C-Bus Commission software allows you to search existing projects.

  1. Click .

  2. In the Project section, enter the name of the project in the Search bar.

  3. The project matching the search criteria is listed in the Projects dashboard.

  4. Select the project and click .

  5. Select Open.

Close a Project

Pre-requisites: The project must already be opened.

  1. Click in the Projects tool bar to close a current project.

IMPORTANT:
  • Trying to close a project while deployment activities are in progress is not possible.

  • Trying to close a project while scanning is in progress is not possible.

Delete a Project

SpaceLogic C-Bus Commission software allows you to switch between the projects. The delete project function deletes a project from the database of the SpaceLogic C-Bus Commission Software.

Prerequisites: The project must already be created.

  1. Click in Projects dashboard.

  2. Click of the project to be deleted from database.

  3. Select Delete. Confirmation pop-up appears.

  4. Click Yes to delete the project.

Import Projects

SpaceLogic C-Bus Commission software allows to import projects and all associated files into the software.

The Import function is available in the welcome screen of the software and in the

To import projects:

  1. Click Import Project.

  2. Windows file browser dialogue is displayed with default location proposed C:\Users\<UserName>\Documents\C-Bus Commission\Exported Projects

  3. Select the project which needs to be imported.

    All the associated project files will be imported (like project file, the eDLT/DLT, BMP and Index TXT files, and so on).

The project files are successfully imported to the software.

Export Projects

Prerequisites: The project must be closed before being exported.

SpaceLogic C-Bus Commission software allows to export project and any associated files from a software as a single file package to save/backup/use elsewhere.

  1. Any project/all associated project files are considered together as a single file package, including but not limited to:

    • Files contained within its project file folder.

      The file package are named/identified as a ".C2Z" file type.

  2. The .C2Z file type are registered with Windows (as per Toolkit .CBZ file type).

  3. You can export the project in any of the two ways described below:

    1. Click of a project in the Projects dashboard and then select Export.

      or,

    2. Right-click on the project in the Projects dashboard and then select Export option.

  4. You can either export the files in C2Z file type or XML file type.

  5. When the export function is invoked, the Windows file browser dialog is displayed with a default name and default location proposed.

    • Default name proposed: 'ProjectName'_YYYYMMDD (where YYYYMMDD is the current date). In the Save as type drop-down list, by default the C2Z files (*.c2z) is selected.

    • Click Save. The file is saved in the default location proposed: C:\Users\<Username>\Documents\C-Bus Commission\Exported Projects.

  6. Select the XML Files (*.xml) option from the Save as type drop-down list to export your C-Bus project to the legacy XML format.

    NOTE: XML format is compatible with legacy Toolkit and C-Gate2 or other legacy C-Bus tools as well as for use with third party C-Bus Enabled systems.
  7. Click Save. The file is saved in the default location proposed: C:\Users\<Username>\Documents\C-Bus Commission\Exported Projects.

    The project and all its associated files are exported successfully from software to the default location.

  8. If you try to export and save a project of any file type to the C:\Users\<username>\Documents\C-Bus Commission\Projects" location, Error pop-up is displayed.

  9. Click OK to close the Error pop-up.

Sort Projects

Prerequisites: More than one project must be created.

SpaceLogic C-Bus Commission software allows you to sort the existing projects. using

  1. Click on Projects dashboard.

  2. Select either Ascending or Descending based on your requirement.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.