Software Version 2.14.0

Add Trigger Groups

The C-Bus Application section allows the user to add Trigger Groups to an Trigger Application.
Prerequisites: The Trigger application must be selected in a created network.
  1. Select a network from the Explorer window.
  2. Click Applications drop down.
  3. Select Trigger.
    Step result: Respective Trigger Groups and Action Selectors section of Trigger is displayed in the Workspace window.
  4. Click in the Trigger Groups section.
  5. Choose address.
    Step result: A Group is created.

    The process to create multiple trigger groups at a time is similar to as demonstrated in lighting application, click here.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.