Software Version 2.14.0

Dimmer Conversions

If there are old dimmers existing in the project, the SpaceLogic C-Bus Commission allows the user to convert old dimmers to digital dimmers.

List of old dimmers that can be converted to new dimmers.

Old Dimmers

New Dimmers

Catalogue number

Unit Type

Catalogue number

Unit Type

L5508D1A

DIMDN8

5508D1D

DIMDD8

L5504D2A

DIMDN4

5504D2D

DIMDD4

L5504D2U

DIMDU4

5504D2D

DIMDD4

To convert:

  1. Open the same project in commission software same as in Toolkit where the dimmer is added in network.

  2. Select C-Bus Devices of the network.

    The available devices in the project are displayed.

  3. Select the dimmer that needs to be converted.

  4. Right click on the Dimmer > Convert Unit.

    Convert Unit confirmation box is displayed.

  5. Select the check box and click OK.

    The old dimmer DIMDN8 is converted to digital dimmer DIMDD8.

  6. When conversion is completed:
    • The address of the dimmer remains the same.

    • The unit type catalogue description and firmware details are updated.

    • The firmware will have the latest version.

    • The serial details needs to be updated manually in property window of the device.

    • The configuration changes made in old dimmer reflects in the new dimmer as well.

      Table below shows the list of properties that will be restored in the digital dimmer DIMDN4 and DIMDN8:

      Properties

      Properties which are restored

      Properties which are not restored

      Project Name

      Project name will be restored as in the old dimmer.

      Not Applicable

      Applications

      Applications will be restored as in the old dimmer.

      Not Applicable

      Channel

      • Group Address

      • Channel Restore Level

      • Power on Delay

      • Min, Max

      Not Applicable

      Logic

      • Logic Groups

      • Assignment

      • Min, Max

      Area

      • Logic Recovery

      • Logic group Restore level

      Learn Mode

      Power Recovery

      Not Applicable

      Enable Burden

      Global

      • Enable C-Bus Clock

      • Enable Local Toggle

      • Enable C-Bus Priority

      • C-Bus Clock

      • C-Bus Priority

      • Local Toggle

      Unit Identification

      • Unit Address

      • Part Name

      • Tag Name

      • Notes

      The Serial details needs to be updated manually in the property editor.

      For DIMDU4, the following properties will be restored.

      • Device ID

      • Kickstart Duration

      • Kickstart Brightness

      • Kickstart Turn On

      • Error Reporting Mode

      • Error Reporting Regular Report Interval

      • Error Reporting Group

      • Error Reporting Trigger group

      • Error Reporting Resend Action Selector

      • Acknowledge All Action Selector

      Along with existing, additional properties can also be configured in the new digital dimmers.

Once the conversion is completed:

  1. Scan the C-Bus Network.

  2. Identify new dimmer on the Network.

  3. Readdress the device to match live network or readdress device to match the project database.

  4. Deploy the device.

Channel Dimming mode (Live Network Sevice)

In Network Device section, right-click on the DIMDDx dimmer unit for Confirm Channel Dimming Mode option.

IMPORTANT: This function is available only for dimmers with firmware version v1.3 and above:
  • The DIMDD8 Dimmer

  • The DIMDD4 Dimmer

This function is disabled while selected dimmer device is in Deployment Queue.

The Confirm Channel Dimming Mode window consists of following information:

  • Dimmer: Displays part name of the unit.

  • Unit Address: Displays unit address of the unit.

Fields

Description

Channel

Displays part name of the dimmer.

Channel Dimming Mode

Displays the dimming mode of the channel.

Channel Status

Confirmed

The channel is not in error status and has dimming mode confirmed.

In confirmed state, both Test and Confirm buttons are disabled.

Not Confirmed

Channel is in not confirmed status when there is no error status, no incompatible load, and dimming mode is not confirmed.

Enable Test button for specific channel, and disable Confirm button for specific channel.

Error

If error exists, specific channel’s Channel Status is updated as error or, as load compatible once the updating channel status is completed.

Ready to Confirm

Test of channel is completed and no errors or incompatible load states exist.

Test Channel

Enable Test button for specific channel and disable Test for other specific channels.

Confirm Channel Dimming Mode

Enable Confirm button for specific channel.

The Channel Dimming Mode Conflicts window is displayed to resolve the identified conflicts as shown below, click Yes to resolve.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.