Software Version 2.14.0

Delete Audio Zone

Prerequisites: Audio application must already be created in the network and Audio Zones must be added.
  1. Select Audio Zone.

    NOTE:
    • A single audio zone can be chosen by selecting the check box of the required group, whereas all audio zones can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one audio zone, then hold down the SHIFT key and select on additional audio zone (grid) using the mouse.

    • For random multiple selection, select one audio zone, then hold down the CTRL key and select the next audio zone (grid) using the mouse.

  2. Click in the Zones section.

    A Confirmation pop-up is displayed.

  3. Click Yes to delete the zones and No to cancel the delete operation.

    TIP: Alternate method to delete selected zone is, right-click on selected Zone > Delete.

Repeat the steps 1–3 for deleting levels.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.