Software Version 2.14.0

Add Zones

Prerequisites: The Audio application must already be created in a network.

Audio application allows to create a maximum number 24 zones.

  1. Click Applications drop-down in the Explorer window.
  2. Click Audio.
  3. Click

    Step result: A individual Zone is added.

    The audio zone table:

    • displays the total number of zones created.

    • can have maximum of 24 zones can be added (0–23).

    • by default, the zone name is ‘Zone X’ (‘X’ is the number of the zone).

    • cannot add multiple zones at a time.

    IMPORTANT:
    • A zone can be deleted during creation/adding itself using “x” as shown below:

  4. The zone name can be modified. Double-click on the zone name, edit the zone name and click enter (or on the empty space of the section) to update the change.
Along with the zone section, the audio application workspace consists of functions of each selected zone and the respective levels of the zone function.

The levels for the zone functions are as below

NOTE: The levels for function are applicable only for below functions.

Zones

Level

Name

Balance

128

Mid Point

Bass

Treble

Mute

2

Amp on, Vol normal, speakers off

5

Amp on, Vol preset, speakers off

7

Amp on, Vol preset, speakers on

255

Amp on, Vol normal, speakers on

Source Number

0

Source 1

1

Source 2

2

Source 3

3

Source 4

4

Source 5

5

Source 6

6

Source 7

7

Source 8

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.