Software Version 2.14.0

DALI Settings

DALI SETTINGS can be performed by toggling on Reconcile Moves Short Address (of Device in Project).

  1. Click > Settings > DALI SETTINGS.

    NOTE:

    While performing reconciliation on DALI devices:

    • If the DALI settings is toggled off, the short address and object Id of a device in Devices in Project section will not be changed.

    • If the DALI settings is toggled on, the short address and object Id of a device in Line Devices section will not be changed.

  2. Select the option from the DALI Device & DALI Line (Line Device section) toggle button behaviour drop-down.

    NOTE: This setting changes the behavior of the toggle off/on button in the DALI Line Device section, making it switch between Off/On at Max Level and On at Min Level/On at Max Level when toggled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.