Partial Push Workflow

A Partial Push workflow in Designer XI consists of the following steps.

  1. Make one or more edits to a design. Any edits are eligible for Partial Push, e.g. install, remove, replace, etc.

  2. Select the edit or edits.

  3. Mark the selected edits for Partial Push in one of two ways.

    • Option 1: Use the Mark for Push button at the bottom of the project pane.

    • Option 2: Right-click the map and select Mark for Push from the click wheel.

    NOTE: Assuming the user has made Partial Push areas visible, Designer XI highlights the selected features using symbology configured in Solution Center.

  4. If necessary, you can unmark edits from Partial Push. Select the element or elements marked for push, right-click the map to reveal the click wheel, and select Unmark from Push.

    NOTE: The click wheel shows up to 8 tools at once. If more tools are available, a context arrow appears so you can cycle through all the available functions.

  5. Select the My Work tab and click the Partial Push button to push the selected areas to the GIS.

    NOTE: Clicking the Partial Push button triggers a warning that actions related to partially pushed areas cannot be undone if you proceed. If you click through the warning, the design is saved and the Partial Push areas are committed to a new GIS session. If nothing is marked for Partial Push, you will receive a warning to that effect.

Once a user initiates a Partial Push, the relevant features are highlighted according to the tenant’s configured symbology for one of three possible states:

  • Push in progress

  • Push succeeded

  • Push failed

At this point, the pushed features are locked and can no longer be edited using the CU attribute pane, the project pane, or the right click wheel. Design components that were not marked for Partial Push are not affected and can continue to be edited, modified, deleted, etc.

The user is now free to make additional edits and may partially push or fully push additional edits (a full push pushes all remaining design features that haven’t already been partially pushed). The subsequent Partial Push always goes into a new session whose name is appended by a corresponding integer in parentheses. For example, the first push for My Session would be called My Session (1), the second push My Session (2), and so on.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?