Abandon from the Click Wheel

As discussed in the previous topic, the Abandon Features tool on the Design tab is a one-click tool. When you click on a gas asset, such as a pipe, it locates the abandon CU for that pipe and the abandon CUs for all connected pipes and other gas features. In other words, it does not just abandon the one feature you click, it abandons all connected upstream and downstream features as well.

Conversely, when you abandon a component using the click wheel, it abandons only that component. It does not trace and abandon beyond the selected component.

To abandon using the click wheel, follow these steps:

  1. Use the Select tool to right-click the component.
  2. On the click wheel, choose Abandon.

  3. Notice, it only abandons that one component.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?