Component Filter

When you click a component directly from the Design tab, the CU Search dialog is already filtered to that component type. In other words, if you click Place Transformer, the CU Search shows you transformers. If you click Place Valve, it shows you valves.

However, when you choose to Search CUs from the click wheel (or use the hotkey Ctrl +F), the CU Search dialog does not initially know which component type you are looking for.

To assist your search, after you type part of the CU code, name, or description, click the desired component type directly in the CU Search dialog.


Electric


Gas


This immediately winnows the list down to only that type.

TIP: The filter is helpful, but it is not required. If you know the code, name, or description of your CU, you can still find it even without selecting a filter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?