Viewing Partial Push Areas

Partial Push areas are hidden by default in Designer XI. To make them visible, click the appropriate button on the toolbar. In the images below, a transformer and two single-phase conductors have been marked for Partial Push.

Partial Push areas hidden:

Partial Push areas visible:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?