Pan to CAD File

This tool is handy if you have already worked with your CAD file using the Move CAD File to Current Extent tool and the Adjust CAD tool. With the CAD now in the correct location, you can pan to it as a quick way to get to your design.


To Pan to CAD File, follow these steps:

  1. Click the CAD that you want to pan to. It highlights in green.

  2. Click the Pan to CAD File tool.

  3. Notice your map re-positions, and the CAD file should be visible.

    IMPORTANT: Can you not see anything? First, ensure the CAD layer is toggled on. Then, try a different basemap. Perhaps the color of the CAD is blending into the background.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?