Hotkeys

Hotkeys are keyboard shortcuts. They are invaluable time savers. Most often, when you have the tool active in the design, it displays its hotkey for future reference.


Map

Map

CU search

Ctrl+F

Save Design

Ctrl+S

Undo

Ctrl+Z

Redo

Ctrl+Y

Zoom In

Ctrl++

Zoom Out

Ctrl+-

Go Back Extent

Alt+LeftArrow

Go Forward Extent

Alt+RightArrow

Deletes Selected Component, CU, or Map Notation

Delete

Cycle through Design Styles

Crtl+Shift+S

Design Tab

Design Tab

Select Tool

Alt+S

Select by Rectangle Tool

Alt+R

Place Work Location

Alt+W

Measure Tool

Alt+M

Place Pipe

Alt+C

Place Generic Line Component

Alt+L

Place Fitting

Alt+F

Place Valve

Alt+V

Place Service Connection

Alt+Shift+S

Place Other Component

Alt+G

Place Cut Point

Alt+Y

Abandon Features

Alt+Shift+A

If on the Layout tab, switch to Design Tab

D

Address Search

Atl+A

Update Catalog

Ctrl+Alt+U

Run Auto-Assign Work Location Tool

Alt+K

Copy current XY location to clipboard

Ctrl+L

Toggle display between projected XY and latitude/longitude

Ctrl+Alt+L

Cycle Through Label Styles when Using the Move Label Tool

A to cycle forward through styles

Z to cycle backward through styles

Design Tab Tool Modifiers

Design Tab Tool Modifiers

Disables Snapping

Spacebar

Snap to line features, but not point features while the hotkey is held

Press and hold e

Finish Linear Sketch

Enter

Finish Linear Sketch

Double Click

Cancels Selected Tool/Action

Esc

Layout Tab Label Placement

TIP: See the topic Label Individual Components to see these hotkeys in action.

Layout Tab Label Placement

Make Label Angle Match the Page Orientation

Press and hold x, then drag with your mouse

Slide Label and Leader Line Along a Linear Component

Press and hold Spacebar, then drag with your mouse

“Unlock” Label Orientation to Set at Any Angle

Press and hold a, then drag with your mouse

Toggle Label on Either Side of a Linear Feature

Tab

Precision Editing Tools

Precision Editing Tools

Line Mode

1

Follow Mode

2

Arc Mode

3

Distance Angle Mode

4

Sketching Templates

Sketching Templates

Rotate Template Counter-Clockwise

<

Rotate Template Clockwise

>

Flip Template Vertically

n

Flip Template Horizontally

m

Lock Template Angle after Rotating (stops nearby lines from overriding your set angle)

Spacebar (press once, do not hold; press once again to unlock)

Enlarge Template (you can enlarge a template to about twice its originally-drawn size)

+

Shrink Template (you can shrink a template to about half its originally-drawn size)

-

Abandon

Abandon

Accepts Abandon CU when Green Badge is Displayed

A

Accepts Abandon CU when Red Badge is Displayed

C

Project Pane

Project Pane

Deletes Selected Component or CU

Delete

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?