Pole

A pole is a support structure used in overhead installations.

Sketching

  • Click in the map to place new poles. Each click adds a pole.

  • Poles do not snap to other devices or conductors. However, when sketching conductors, they snap to existing poles.

  • Poles can also snap to guide points for precision placement.

Deletion and Removal

Poles support both deletion and removal via the Click Wheel. Delete is the preferred tool, but Remove is offered as a legacy option for some customers to support custom workflows.

  • Use the Delete option to delete designer-sketched poles from a Design.

  • In certain unusual cases, use the Remove option to flag a pole for removal. This is rarely done and only makes sense for specific workflows in which a customer’s GIS is missing a pole intended for removal.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?